Hello,
Today I just installed QSPICE on my Windows 10 laptop, and what I can see is that when I run the simulation (meaning when I press the green Run button) the schematic is resizing (becomes smaller, like when the restore down button is pressed). Is this the default behaviour of the QSPICE?
Why this is happening?
Before running the simulation - in this case the schematic window is put on the whole screen:
After running the simulation - in this case the schematic window is resizing automatically, becoming smaller, like someone is pressing Restore Down button:
Yes, that is the intended behavior. When you run a simulation, the schematic comes out of full screen mode because there will be a waveform window to see, too. If I don’t do that, some graphics card drivers give a very corrupted view of the new window that shows up. The current behavior circumvents a bug in some GPU drivers.
–Mike
Ok. Thank you for clarification. I thought that it was something from my side for this behaviour (my laptop, or whatever something that interferes at me and shows such behavior).
If you use windows, a solution to this for me was to use PowerToys fancy zone feature to create a window that fills my screen, but does not actually put the window in a maximum state for the UI’s sake. After this, QSPICE will remember your window size, so you really need to only do it once in a while.
1 Like