Hello,
Im trying to run the library and test the examples, as i mencioned on the tittle im using stm32cubeide, i made a port based on the project EVK3000_F429_CubeMX.
I followed this guide to import correctly the library to the project, works fine i think: System Hardfault when calling dwt_probe() - #9 by bruno
I used this code to test the spi conections and work fine:
when i test the ex_00a_reading_dev_id example, the dwt_probe() return -1(ERROR) and then dwt_readdevid() jumps directly to hardfault_handler. I can confirm that dwt_probe uses the readspi function implemented:
idk whats happening but what i understand is that when it enters hardfault, its because of memory access error, idk what am i missing.
Thanks in advance for response.