I am integrating our Cortex-M33 MCU board with DM3000 EVB (DWM3000EVB - Decawave) in IAR IDE project
Our MCU signal is 1.8V while DM3000EVB uses 3.3V signal, so I add volt level shifter in between.
Currently, I got system hard fault when it calls dwt_probe().
Here is my software setup:
1- I added this to the IAR linker script to place dwt_driver APIs in flash:
define exported symbol __dw_drivers_start = 0x08001180;
define exported symbol __dw_drivers_end. = 0x08008FFFF; //512KB
define region TEXT_DW_region = mem:[from __dw_drivers_start to __dw_drivers_end];
define block DW_DRIVERS with alignment = 4 { section *.dw_drivers};
place in TEXT_DW_region {block DW_DRIVERS};
2- I link the project with libdwt_uwb_driver-m33-hfp-6.0.7.a library
3- I run read_dev_id example
4- I probe 3V3 SPI signal on the DM3000EVB side and see it outputs DEV_ID correctly when dwt_probe() calls my platform-specific readspi() function. Then I see it does not exit dwt_probe() but jumps to hardfault handler forever.
I read DW3XXX_Software_API_Guide_2p2.pdf document to see it mentions about populating “struct dwt_driver_s dw3000_driver” but I do not see such structure defined in the example code for STM32F429 Nucleo EVK or nRF52840 EVK
Should I need to populate “struct dwt_drivers”? Can you provide a example about populating that structure?
Can you write your own code to test your SPI layer, at least as far as reading DEV_ID? I just want to make sure that you’ve got things like the SPI mode set up right. Specifically, if you push five 0x00 bytes, you should get 0xDECA0302 back for the last four.
The second problem is that you specify the address of the end of the __dwt_driver_end symbol.
The way dwt_probe() is organized is that there is an iterator of N driver structures, so you read chip id via spi, then compare to the driver struct, if matches - use that driver.
One problem is that if spi does not read correct chip id.
Second problem is that say if we reach the final N driver struct, the dwt_probe() will keep iterate and that obviously would end to an error.
I would recommend you dump the downloaded code and check memory where drivers structs placed.
I confirmed that dwt_probe() calls our platform-specific spiread() implementation and I also probed SPI lines to see that DM3000 returns correct CHIP_ID which is 0xDECA0302.
The second problem is that you specify the address of the end of the __dwt_driver_end symbol.
Second problem is that say if we reach the final N driver struct, the dwt_probe() will keep iterate and that obviously would end to an error.
I do not understand what “driver struct” here. Do you mean “struct dwt_driver_s dw3000_driver”?
Should I need to implement such structure in the code? I do not see any reference implementation for that structure in DWM3000EVB_Release_v1.2.zip file that I downloaded on Qorvo website.
Can you explain more about driver struct and how to support it in new MCU platform?
I can resolve the issue now.
I need to place this section at the address in flash specified by __dw_drivers_start in IAR linker script:
define exported symbol __dw_drivers_start = 0x08001180;
define exported symbol __dw_drivers_end. = 0x0800119F;
define region TEXT_DW_region = mem:[from __dw_drivers_start to __dw_drivers_end];
define block DW_DRIVERS with alignment = 4 { section .dw_drivers};
place in TEXT_DW_region { block DW_DRIVERS};
Now I can some examples fine.
Thanks for the support. I will post questions when I evaluate more DM3000 features.
Hi @BenFossil, thanks for the description of how-to link the ABI drivers’ library in IAR. That also shows that the EABI is a working mechanism, which is great.
A contribution to people who use STM32CubeIDE (I don’t know way Qorvo does not explain this in the API guide !!! )
Add in the linker script what is told in the API guide
/* The program code and other data into “FLASH” Rom type memory /
.text :
{
. = ALIGN(4);
__dw_drivers_start = .;
KEEP((.dw_drivers))
__dw_drivers_end = .;
Do not include the static library in the regular way, IT WILL NOT WORK! Do this instead (in my project I am using M4 core so I picked the suitable API library) Image2|565x500 Image1|690x441
So you leave Libraries (-I) empty BUT in MCU G++ Linker Miscellaneous you add in “other flags” what is shown in the picture (remember to use a suitable API library for your core)