copy this and paste into the schematic at QSpice:
«line (9400,-13600) (8950,-14100) 7 0 0xa0a0ff -1 -1»
«rect (8750,-13500) (9200,-13950) 0 7 0 0xc0c0 0xff92 -1 0 -1»
«ellipse (9400,-13600) (9150,-14100) 0 7 0 0xa0ffa1 0x96c0 -1 -1»
«arc (9250,-13950) (8950,-13250) (7950,-13200) (8700,-12800) 0 7 0 0x1000000 -1 -1»
«arc3p (9100,-13600) (9700,-13650) (9400,-13400) 7 0 0x9dc000 -1 -1»
«triangle (9300,-13550) (9050,-14100) (9150,-14150) 7 0 0x528000 0xffff00 -1 -1»
«coil (8650,-13650) (9400,-13800) 0 7 0 0xc000ff -1 -1»
«zigzag (9300,-13400) (9100,-14150) 0 7 0 0xff57d2 -1 -1»
«component (10100,-13700) 0 0
«symbol
«shorted pins: false»
«line (300,150) (-150,-350) 7 0 0xa0a0ff -1 -1»
«rect (-350,250) (100,-200) 0 7 0 0xc0c0 0xff92 -1 0 -1»
«ellipse (300,150) (50,-350) 0 7 0 0xa0ffa1 0x96c0 -1 -1»
«arc (150,-200) (-150,500) (-1150,550) (-400,950) 0 7 0 0x1000000 -1 -1»
«arc3p (0,150) (600,100) (300,350) 7 0 0x9dc000 -1 -1»
«triangle (200,200) (-50,-350) (50,-400) 7 0 0x528000 0xffff00 -1 -1»
«coil (-450,100) (300,-50) 0 7 0 0xc000ff -1 -1»
«zigzag (200,350) (0,-400) 0 7 0 0xff57d2 -1 -1»
»
»
What I’m interested in, is the translation procedure from the text that is actually written in the .qsch file for the text attributes, and what appears on the schematic when it’s displayed by QSpice’s schematic editor, so when I generate the .svg, the text will appear the same as in QSpice’s schematic editor.
Edit: I missed the first line in the code above. Now it’s correct.