I have a third party mosfet provided as a .subckt file.
I have copied the normal mosfet symbol, replaced the library file and used symbol type X and it seems to work fine.
When implementing this in a model, I cannot plot the losses P(M1) which is normally available for a mosfet modelled as VDMOS model
Drain and Source currents are also not available without extra resistors.
Hi, I saw also this problem with not being able to see the drain/source currents and power with third party mosfet. I am not sure why is so, and if this should be like that. As a workaround is what you said by putting extra resistors for reading the drain and source currents or by putting a voltage source of 0V to achieve the same thing.
Hi, I am also facing the same problem not able to see the current and power waveforms for 3rd party subcircuit models. I am not able to fix it. For LTspice the 3rd party models are working with current and power waveforms.