Hi,
Can we all contribute to develop a workflow for modelling an op amp from datasheet parameters in Qspice? I am asking this, because most of the vendor spice models are developed in TINA or Pspice or LTspice which is having issues with QSPICE.
Regards,
Heisenberg
I see a distinct lack of enthusiasm for this enterprise. I think I know the reason, but I’m curious to know if there might be more than one.
You should check out this:
Simulating op-amps presents a paradox. While SPICE excels at transistor-level simulation, op-amps are designed to hide transistor limitations in order to behave more like an ideal op-amp—making it a challenge to create a robust, simple, SPICE model...
It makes Rail to Rail Op-Amp modeling a solved problem.
–Mike
2 Likes
Hi Mike,
Thanks for the explanation.
But in the Qspice Op amp model, where we can add output impedance vs frequency?
I believe this is an important parameter for stability analysis.
Regards,
Heisenberg
1 Like
i have same problem thanks for solved the problem
Mike,
The link to your Op-Ed is dead. Do you have an updated link?
Belov
April 10, 2025, 12:36pm
7