Hello,
I’ve an Issue where I use the native zener symbol with this subckt:
The issue is that I’m unable to probe the current through the subckt, but if I place a zener without a subckt attached to it I can.
I think it may be a general issue with this symbol and subckt. Because it works fine to probe the current through the subckt if I just take the default symbol created for the subckt.
.SUBCKT esd9x3.3st5g 7 1
**************************************
* Model Generated by MODPEX *
*Copyright(c) Symmetry Design Systems*
* All Rights Reserved *
* UNPUBLISHED LICENSED SOFTWARE *
* Contains Proprietary Information *
* Which is The Property of *
* SYMMETRY OR ITS LICENSORS *
*Commercial Use or Resale Restricted *
* by Symmetry License Agreement *
**************************************
* Model generated on May 6, 06
* MODEL FORMAT: PSpice
* anode cathode
*node: 7 1
* Forward Section
D1 2 1 MDD1
.MODEL MDD1 D IS=5.85762e-16 N=1 XTI=1 RS=0.5
+ CJO=8e-11 TT=9e-10
* Leakage Current
R 1 2 MDR 9.85075e+06
.MODEL MDR RES TC1=-0.00450549 TC2=0
* Breakdown
RZ 2 3 0.477685
D3 4 3 MDD3
.MODEL MDD3 D IS=2.5e-15 N=0.5
EV1 1 4 6 8 1
IBV 0 6 0.001
RBV 6 0 MDRBV 5600
.MODEL MDRBV RES TC1=0.00022
D4 8 0 MDD3
L 7 2 1e-15
IT 0 8 0.001
.ENDS esd9x3.3st5g.