How to Install Qspice on Linux

How to Install Qspice on Linux

  1. Create a bootable USB drive with Windows PE (Preinstallation Environment)
    You can use Ventoy to copy the Windows PE ISO image to your USB drive.

  2. Install Qspice on the USB drive
    After booting your computer from the USB drive using Windows PE, install Qspice directly onto the USB drive. Then, run Qspice and apply the Qspice update if available.

  3. Copy Qspice to your Linux system
    After installing, reboot into Linux. Then, copy the Qspice installation folder from the USB drive to your Linux hard drive.

  4. Run Qspice using Lutris
    Use Lutris to run the Qspice executable. Follow the setup based on the configuration examples provided.

**** Lutris configuration screens Click here: Imgur: The magic of the Internet

How to Update Qspice

To update Qspice, simply repeat the same process:

  • Boot into Windows PE.
  • Reinstall Qspice on the USB drive and run the update.
  • Copy the new installation over the existing one on your Linux hard drive.

Done! Qspice will now be up to date.


Note about the Qspice Installer

The main issue with this process is that both the Qspice installer and updater perform strict checks on the operating system, requiring Windows 10 or 11, 64-bit.

Because of this, Wine is unable to “trick” the installer, and Qspice cannot be installed directly on Linux.

It would be much more practical if the developers simply showed a warning about the recommended Windows version, instead of blocking the installation entirely. That way, Linux users would be able to install and update Qspice more easily.

For those interested in experimenting with QSpice on Linux: Another option is to use Codeweavers’ CrossOver (version 26 onwards).

This very short video illustrates the steps demonstrated on Debian 12 64-bit (Bookworm):
HowTo install QSpice on Debian 12 with CrossOver-cxOffice-v26

This set-up works on AMD64 real HW, as well as in a VirtualBox Virtual Machine.

Known issues as of now:

  • Graphics issues with qraw windows, refresh on resizing does not always work properly, cursors are not displayed
  • Crash in Virtual Machine, if Graphics Mode “DXVK” is selected (something that was not seen with real HW)

If this “known good” set-up works on your machine, chances are that QSpice would also work under Wine 11.x or one of its other derivatives.

Please note that I am not affiliated with Codeweavers; any issues found should be addressed in their forum and/or their support.

I hope this helps.

1 Like

Hello @MadDog, @rdepaoli

I only saw this today, after @rdepaoli replied. I’ve already said you can use Qspice almost flawlessly in Linux, see this.

Vlad