Is there any way to see what “Feature Requests” have been accepted onto the “To Be Implemented” list? I’ve seen (and requested) several features that would make my job easier, but I don’t want to irritate the team by asking about the implementation schedule (or whether the feature request has been rejected).
Thanks,
Carl
3 Likes
Good suggestion…
Hope the Qspice team can put this request on the top…
+1
Has there been any movement on this?
I would like to add:
the option to move degree axis from right to left, when only plotting phase
and:
add horizontal lines in phase plot when only plotting phase
as well as:
add ‘‘minor’’ vertical lines in log plots
to the list.
Another thing that would be nice would be:
simplifying frequencys in plot winow (ie. displaying 1 kHz instead of 10^3Hz)
based on Flipped phase plot in ac analysis I would like to add:
add bode style negative phase values to right side axis in the graphe window
to the list, please.