Hi,I am now using DWM1001C module and Firmware_Image"DWM1001_PANS_R2.0.hex" it works well, so I want separate DWM1001C use NRF52832 and IC-DW1000, I want add PA and LNA,between the antenna and the DW1000
I found in “APS004_Increasing-the-Range-of-DW1000-Using-LNA_v1.6” and “APS009_Operating-the-DW1000-under-LAES-regulations_v1.4” ,when use PA and LNA,some GPIO and some Register must be use to control the DW1000
So how can I use DWM1001_PANS_R2.0-API to control it?
Thanks a lot
Hi! I’m confused too about routing anchors.
It is my understanding from DWM1001_System_Overview (figure 2) that Bridge Nodes obtain Tags positions from the Tag itself during Group Poll Messages (not from the anchors). From the whole document and Message descriptions I would say that that’s true.
We want to use MDEK1001, which is applied to the range of 1kmX1km outdoors. Do you have any suggestions on how to use it?
Our application is personnel positioning, and there is a distance between upstairs and downstairs
Hello,
We bought MDEK1001 kit to see what UWB was able to do and now we want to make a demo
What we need to do for the demo: add a read/write characteristic in the BLE advertized service to be able to access the user data seen in the API guide and modify the Android application to access the user data through BLE.
I understand that PANS is shipped as a library/binary only.
If I’m not wrong, the BLE service advertized by the nodes is in PANS so I believe that a characteristic can’t be added to the existing service.
But do you think that it’s possible, in the application part, as in dwm-api-test, to define another service with this read/write characteristic to access user data ?
I believe that PANS is using code that is in SoftDevice part to create the existing BLE service, is it possible to use as well the s132_nrf52_3.0.0 API (SoftDevice header files) to link to SoftDevice part and do this new BLE service ?
And can we make it be advertized as well as the existing one, the one that is in PANS library ?
Feel free to let me know if I’m wrong somewhere in my understanding
Hi Taylor,
Please find the new link here as Decawave is now part of Qorvo : DWM1001C Product Overview
In the Documents Tab you will find all related documents.
The initial post here shared the name of the file:
“/DWM1001/Factory_Firmware_Image/DWM1001_PANS_R2.0.hex”
I have downloaded hundreds of files from the Qorvo website, including, I think, all of the zip files. The hex file that is mentioned in the initial post is missing.
The DWM1001 is utterly worthless without this file. It ships from Qorvo with no firmware - until it is flashed with this file, it looks pretty on a desk and is capable of absolutely nothing.
As I post on another part of the forum I have the PANS_R2.hex so if you want it, just send me a private message with your email address. And I will send you the file. (I can’t upload a .hex file on the forum)