Hi all,
I tried to setup the DWM1001 gateway in the Raspberry Pi 3 Model B V1.2 but failed. When I insert the sd card(Tried with 8GB and 16GB), the led blinks for a while, but thats it. There is no led blinking in the network port as well. Can anyone please help me with this issue?
Thanks in advance.
Hi Kasun,
Are you using the image provided by Decawave and did you follow the Gateway quick deployment guide ?
Do you have any other 16gb or 32gb sd card to test with ?
Thanks
Yves
ramg
August 23, 2019, 3:41pm
3
The image provided by Decawave doesn’t work in 16gb cards.
See:
Hi programonauta, the model is RB 3B and didn’t try with 32GB, maybe I will today.
The image has two partitions. The boot one with no problems, and the Linux one. I cannot mount the Linux partition, in a Linux distro using:
mount -o loop,offset=50331648 ./DRTLS_raspbian_R2.0.img /mnt/raspbian/
Output:
wrong fs type, bad option, bad superblock on /dev/loop0,
missing codepage or helper program, or other error
I think the problem is on the image file.
Downloaded from https://www.decaw…
Hi Yves and ramg,
Thank you for your replies.\
@Yves_Bernard_Qorvo Yes I am using the decawave img and following the quick deployment guide. I will try it again with a 32gb card and get back.
@ramg Yes I saw the same in few other posts. Will try it on Monday.
Thanks people
1 Like
FYI. I use a 16GB SD card and it works for me.
Below are the exact products
The SanDisk Ultra microSD UHS-I card gives you the freedom to shoot, save and Share more than ever before. It is perfect for recording and watching Full HD video,(2) with room for even more hours of video. Transfer speeds of up to 100MB/s help you...
$13.99
Follow up on my question.
I used a 32GB sd card today. The image worked fine in it.
1 Like