Hello,
I have a question regarding the DW1000 IC in combination with a TCXO and would be forever grateful if Decawave or someone else could comment on this question.
I would like to use a TCXO in order to drive the DW1000.
It has already been discussed in this thread that the data sheet does not mention the input impedance of the XTAL1 pin:
The only information regarding the requirements for an external clock given by the date sheet is shown below:
Decawave can you tell use the input impedance (R & C) of the XTAL1 pin?
The datasheet recommends the TCXO “ASTXR-12-38.400MHz-514054-T” which has an output load impedance of 10K || 10PF.
Is 10K || 10PF the input impedance of the DW1000 XTAL1 pin?
I also would like to know if the DW1000 can be driven by LVCMOS instead of clipped sine wave?
In addition, I saw that ABRACON recommends an AC coupling capacitor with a value larger than 1nF:
Decawave recommends to use an AC coupling capacitor of 2200pF.
Why exactly this value?
I saw that some TCXO manufacturers recommend an AC coupling capacitor of 0.1uF.
Which value should be used in this case?
How can the value of the coupling capacitor be properly determined?
Will a value of 0.1uF which is much larger than the recommended 2200pF do harm?
Lastly, I also saw that some manufacturers recommend a termination resistor, but I don’t think that this is really necessary if the TCXO is right next to the IC. What do you think about this ?
Kind regards
firstdragon