Zero distances when two modules communicate

Greetings, everyone!
Sometimes when communicating between two dwm1000 modules I get zero distances or for example four digit numbers instead of normal distances (the modules are not more than two meters apart).
Can you tell me what the problem could be, I read somewhere that about 1% of packets may be broken or erroneous, but is the result then zeros?
As I found out, it’s because I lose packets, i.e. the transmission happens, but there is no reception, and it can be both unsuccessful reception of INIT packet and unsuccessful reception of END packet, usually reception of RESP packet happens normally.
I use two dwm1000 and two stm32L151.
С уважением, Кирилл.