I read in one article that microcontrollers are planned for introduction to QSPICE eventually. Is this ever going to be possible? Thanks.
Because QSPICE can compile and simulate Verilog, it’s well-suited to simulate a microcontroller. I’m waiting for someone to take a RISC-V core from Github and spin it up in QSPICE.
Fantastic. I’m guessing we won’t see any commercial MCU’s unless the Verilog code is open source.
I agree- you won’t see a commercial MCU’s Verilog source in public (at least, you shouldn’t). But, there are a good number of open-source processors out there that can be a good starting point. For example, there are plenty of RISC-V examples available, plus older architectures like 8051 if you just need a simple 8-bit processor.
Well, in QSPICE Verilog code is translated to C++ which in turn is compiled to native x86 executable code (DLL). So it should be possible for microcontroller vendors to build a pre-compiled DLL for QSPICE, thus not revealing the internals of the microcontroller, shouldn’t it?
Absolutely.
Should also afford higher performance than a Verilog-based implementation.
–Mike
Has anyone done this yet? I may have missed it. Thanks.
Hi, David.
You might want to see the QMdbSim project on my GitHub repository. It uses the Microchip simulator as a backend to run microcontoller programs within a QSpice simulation.
–robert