Recently, I encountered a thorny problem. Neither the software nor the hardware has changed, but 10% of the cards produced do not measure distance or the success rate of measuring distance is only half of the original. I found after test that the waveform of the continuous wave mode is the same as that of a good card when it is first powered on, but the waveform changes a few decades after it is powered on. The UWB schematic diagram of the card is as follows:
The waveform of continuous wave mode in the first ten seconds after power on is as follows:
The waveform in continuous wave mode is as follows ten seconds after power on:
Who knows what causes the spectrum waveform change?
Thank you in advance!