Hi, we changed from regular crystal to TCXO after experiencing some issues with crystal frequency previously.
We are now using JT21G However, when we use the recommended capacitor value (2200pF) for TCXO from dw3000 datasheet, with 1.8V VDD_TCXO, we cannot get the 800mV amplitude required by dw3000.
We just want to know what’s the official recommended TCXO for dw3000 now and where we can buy it? The recommended ones on the datasheet are no longer available.
there are some changes in the datasheet and we would like to know something that has been definitely demonstrated to work with dw3000 and is still manufactuered
here is the schematic for the TCXO part in our design
It`s based on KCL/KVL
Think how 2200 pF value was obtained.
And JT21 is a bad choice. Vout=0.8V (min)
DW3000 need V=0.8V (pk-pk, min). There is no any margin.
And voltage at DW3000 will be always less then Vout, because C11 and R11||R10 form divider.
But you can not remove R10 and R11, because they provide DC bias for AC-coupled signal.
P.S.
You can try remove R10, R11 and replace C11 with resistor (0 to 10-33 Ohm).
No idea how long trace is… But this is fix for lab. usage, not good for production samples.
These recommended parts are also both obsolete and there is no stock available.The JT21 was selected based on the properties of the datasheet-recommended TCXO.If the JT21 is a bad choice, then what is a good one?