Hi, What communication interfaces can PAC52xx support?
Hi Winter,
The serial peripheral content within our family of PAC52xx devices is as shown below:
ARM Cortex M0 based PAC52xx:
- UART (Qty 1)
- I2C (Qty 1)
- SPI (Qty 1)
If you look at the PAC55xx family of devices then it would look as below:
ARM Cortex M4F based PAC55xx:
- UART (Qty up to 3)
- I2C (Qty 1)
- SPI (Qty up to 3)
- CAN 2.0 (Qty 1)
Hope the info helps!
can you share the sample code of controlled area network extended version with pac25140?
Hi Nikita196, and thanks for joining the forum! Currently PAC2x140 BMS parts are not supported by the forum yet. Please send your question to: appsupport@qorvo.com
Qorvo Team
The PAC52xx series supports UART, I2C, and SPI interfaces, with one of each available. If you’re looking for more advanced communication capabilities, the PAC55xx series offers up to three UARTs, three SPIs, and additional CAN 2.0 support. It’s good to keep in mind which specific interfaces you need for your project to choose the appropriate family.