Wb003 uwb pcb antenna

Hi,
While we can certainly adjust the transmission line width based on impedance calculations, I’m unsure whether the antenna feeding point (marked as (1)) is considered part of the antenna structure or the transmission line. Can we modify its width as well? Unfortunately, there is no further documentation explaining this.

For context, model wb001 features a wider transmission line (utilizing a microstrip and accounting for the stackup), but it results in a slightly higher antenna profile compared to wb003. This makes me curious if we can optimize or rearrange section (1) in a similar way.

Please refer to the attached file for details.

The simplest approach would be to considered the feed point part of the line and adjust the line width to 50Ω impedance.
The WB001 example is on double sided 0.8mm FR4, hence the wider line. The WB003 example is taken from the DWM1001C module which uses a multi layer stackup and CPW line. WB001 is larger because it covers more channels (Ch2 to 5), whereas WB003 on DWM1001C needs to only cover Ch5.
To use either in your own design, the best approach would be to use EM simulation to adjust placement and feed line impedance according to your stackup.