Hi, i im new to QSpice and would like to ask if is possible to add negative value to DC Source, as i im trying to simulate TTrak temperature output bias and need negative value from VSVC.
Here on schematic it is labeled V3 and value is -1.8V (i need to have negative value to bias output stage current to cca 150mA).
Simulation gives me error and would not run, if i put 1.8V for DC value then simulation runs but output stage is not biased as it needs -1.8V.
How to add to voltage source negative voltage? In this example -1.8V?
Here is project with models as forum does not allow me to attach files.
Your link goes to a sign-in page, not to something I can view. So, I’m just guessing… Is this what you’re trying to do? If not, maybe fix the link so that we can access your example.
@ronovar Increase your trust level to Basic User by completing tasks in this post. Increase forum trust level
As a basic user, you can upload a file to the forum (it appears that the forum has recently implemented filtering, so your file may be delayed by a day if this is your first upload, to prevent spam).