UWB latency in positioning

The latency isn’t inherent in UWB, it is a result of the protocol and firmware used for calculating the position. So while it can be reduced getting it down to something suitable for real time control is tricky, you can’t do it using the out of the box code supplied. You would be looking at creating your own firmware for the system.
But if you were to do that then it is possible.

Warning: blatantly commercial plug
Or you could buy one off the shelf.
We have a system that will give 100Hz positions with fixed latency of 60ms.
Here is a video of using it to steer a car https://vimeo.com/363324210
And here we are using it to position a camera and then in real time use that data to move the camera in a virtual world https://www.youtube.com/watch?v=UqX9_OetZRY

2 Likes