I’m very new to the decaWave system. For my current project my team and I have bought the DWM1001 modules. Currently, the system has a maximum update frequency of 10Hz. Is the 10Hz limited to physical component constraints, or can this be increased by altering the firmware on the modules themselves? Any help and information is greatly appreciated.
The PANS FW which comes with the module has this limitation. If you build your own system, then it depends on lots of things: message frame lengths, MCU/SPI speed, RTLS protocol used, number of devices that need to work in the same environment etc.
Moving TREK1000 to a product is a good doc to read on this.