Hi all,
I’ve been characterising the Decawave ranging device kit (TREK1000) in a motion capture room to try and determine its accuracy. The set up is as follows: A0 (0,0,0.77m), A1 (0,1.5m,0.77m), A2 (1.5m,0,0.77m), A3(1.5m,1.5m,0.77m) - anchors placed upon tripods in a large, empty room. All these coordinates are within +_1mm (as validated using out motion capture software). The tag then begins its journey from approximately (6m,6m,0.1m) and travels towards the middle of the enclosed square (defined by the four anchors) along the ground (maintaining a height of ~0.1m).
As expected, the x-y plane position estimate is accurate, to within +_ 0.2m (which improves when the tag enters the enclosed area). The z-axis position estimate is much worse, about +_ 1.5m, improving substantially when the tag enters the enclosed space. During this ~60s data collection period, we made ~600 measurements. Of these 600 measurements, about 40 were NaN (null measurements).
Curiously, when I raised anchor 3 (A3) out of plane to (1.5m,1.5m,1.2m), the accuracy didn’t improve (although the z-axis ambiguity was lost), but the number of null measurements increased dramatically (of the ~600 measurements, ~300 were null measurements). These null measurements only occurred when the tag was close to the ground (well below the anchor plane, and did not occur when the tag was at the same height above the plane).
Does anyone have any idea why the number of null measurements increases so dramatically when the fourth anchor is raised out of plane? I’ve attached the figure and data for this test.
Thanks for your help.