Hi all,
I purchased two DWM3001CDKs in hope to transmit data via UWB/Impulse Radio. One of the boards should act as the transmitter while the other is a receiver. Now, I have checked the SDK folders and peripheral examples etc. However, I have not found a way to transmit via the UWB antenna on the UWB chip which can be addressed via SPI from the Nordic MCU (due to the datasheet). As far as I am concerned, the examples given in the examples folders are using only the Bluetooth antenna on the MCU.
Has anyone tried data transmission via the UWB chip yet and could offer me some guidance on where to look into in the code?
I would be thankful for any kind of help!
Kind regards!