I’m new to working with electronics and I’m trying to control a high-side N-channel MOSFET. I’ve encountered an error in my circuit. Could someone please help me solve this problem?
See
IR2101.qsch (11.4 KB)
Parent.IR2101.qsch (16.6 KB)
IR2101.qsym (1.2 KB)
Thank you alot, you’r my hero
I understand now ![]()
@bordodynov provided you with a behavioral model of the IR2101. You can also run the Infineon Pspice model from Qspice. Here is a replication of the Infineon demo circuit in Infineon-IR2101-PSpice-SimulationModels-v01_00-EN.zip
Two major things to pay attention to:
- In the Infineon demo circuit, its VCC source is a ramp source. This Pspice model seems to require a 0V VCC voltage at t=0 for this simulation to work. A direct DC source will fail this simulation.
- Possibly related to multiple formulas in the IR2101 model, 80-bit math (disable fast math) is required for Qspice to run this model.
In any case, a behavioral model will be much easier if you have no special concerns which MUST use the Pspice model from Infineon.
Parent.IR2101.qsch (25.3 KB)
IGBT_650V_TRENCHSTOP5_F5_L1.txt (50.8 KB)
Diagram from Infineon-IR2101-PSpice-SimulationModels-v01_00-EN.zip
Thank you so much. This is exactly what I needed to know. Thank you again
![]()
Also feel free to arrange symbols like the application schematic, and follow conventions for making schematics. Makes it easier to spot errors.