Hi
Is there a way to set the time when a PWL file source will start to be active?
( A start delay of the PWL file data )
If not I suggests adding a time parameter at the end of the PWL file definition for this purpose.
Best regards Håkan N
Hi, Honeybee.
Can’t you change the PWL file to delay the start of the data changes?
–robert
Hi,
I always use a transmission line to delay the start point of PWL data. When comparing experimental data with simulation data, I employ this method. You can adjust the timing of the PWL data in the schematics without having to modify the PWL file.
2 Likes
Hello,
the behavioral voltage source supports the delay function which purpose is actually to delay signals in time. I have tried for the PWL source and it worked well.
2 Likes
Hi,
Amazing! I completely overlooked that. Thank you.
Hi WinterMime
Thanks for your hint. That solves my problem.
Many Thanks.
Håkan N