Is there any concern / trade-off with operating the TGM2635-CP at a lower quiescent current, closer to 750-800mA?
The TGM2635-CP has not been tested by Qorvo at quiescent currents this low. There will be effects like reduced linearity. What are you trying to achieve by reducing quiescent current to 750-800mA?
Thank you Chris. I am lowering the quiescent current to reduce the small signal gain of the amplifier. This is currently the least physically invasive option for an assembly.
Yes you would get lower small signal gain. There will be quite high variation in small signal gain between devices and across temperature, so worth taking this into account.
Hello Chris,
Hope you are doing well.
I am seeing variation in the P_Sat of the TGM2635-CP for device to device for the exact same setup (at room temperature, with recommended Q-point baising). It is almost like:
Device-1 : Pout = 49.57dBm
Device -2 : Pout = 49.69dBm
Device-3 : Pout = 50.3dBm
Can you please help me with the following queries:
- The above mentioned power values are the maximum power and it is reducing as we go above in frequency, is this type of shift ( around 0.7dB) in output power level expected in device to device variation?
- The drain currents are different for the amplifier IC. Is it mandatory that the IC should take around 11.5A as per datasheet to give the expected P_SAT or can there be difference in that value?
Thankyou so much for your time and support. Looking forward to hearing from you.
- Kind Regards
Sorry for the delay. To support your questions it would be best if you could e-mail appsupport@qorvo.com stating your company name and location. Then your regional applications engineer can assist further.