Testing tramsmission without reception

Before I begin to build the second board with DWM3000, I would like to test the right transmission of the first one I just finish.
Due to the routines I wrote for the accces to the registers of the device, readings and writings of the registers are successfull without errors.
After configuration of all the registers, I am intending to test a transmission without the waiting of response. I configure the crucial parameters of the MAC Header of the frame like this : Frame Type = DATA, Frame Pending = 0, Ack Request = 0, Frame Length = 75 bytes. Fast command : CMD_TX
Is it possible to control the right emission of the frame through the GPIO3 configured as 001 for operation as TXLED output?
Thank you
GOFFIN David
Regulation-Mesure