I have the MDEK1001 with 3 anchors, 1 tag and a listener. I’m connected to the listener via USB and use “lec” in the command. I’m seeing the anchor x,y,z locations update but there can be lag of 1-3 seconds before I see the coordinates update. It doesn’t make any difference if I have updates of 10 Hz or 5 Hz, etc. I realize the location calculations take some time at the tag but is there any way I can speed that up? Our application requires an update as soon as possible but more importantly it needs to be predictable. Any help would be appreciated.
Hi rkeiner,
You shouldn’t observe such a long delay.
The tag can be set with two update rates, one for stationary and one when it is mobile. Have you tried to set both to 10hz ?
Thanks
Yves