Hi,
I intend to design a system using MDEK1001 devices. I believe I will use at least 6 anchors (to ensure LOC) and 10-12 tags. The area I intend to cover is 30 x 30 meters. From my understanding, to get the position of each tag, one can use BLE on the tags to transmit the data packets to the BLE receiver (android device). I have the following questions for this design idea.
- Do you think BLE is a reliable option given the numbers and amount of tags?
- Can you setup Gateway to receive data through anything other than BLE? i.e UWB?
- If I had to put a sensor on the tag and sensor could communicate via I2C. Can I use existing nrf52 processor and use PANS library to access that sensor or put another nrf52 board to read DWM1001 and send data via BLE?