When first selecting a symbol from the Symbols & IP browser and moving it on the canvas, the symbol doesn’t rotate when using CTRL+r. Once the symbol is placed once, CTRL+r works as expected on the second instance. Until a new symbol is selected, then the same thing happens again for the new symbol.
Humm, that’s not the operation that I see. Ctrl-R works when dragging a part from the Symbol & IP browser. I’ve never seen that not work.
Ah, I was not aware you could drag the item. The bug only seems to appear when selecting a symbol via double clicking.
A cool stuff, you can drag schematic (.qsch) and symbol (.qsym) from file explorer to schematic. It is very convenience especially for user created symbol.
When a symbol is double-clicked in the Symbol & IP Browser to be placed in a schematic, it can only be rotated after the first symbol has been placed (maybe the input focus is not on the schematic yet and still on the browser).
Ah! I forgot I implemented double click as a way to initiate a drag. OK, double click is no longer a 2nd class citizen and it works as well as simply dragging.
Thanks,
–Mike
Thanks, Ctrl+R
works now. Maybe Ctrl+M
should as well?
It’s Ctrl-E for mirror.
Ctrl-M is reserved to putting a new line into a piece of text on the schematic.
–Mike
Oh, I see… Funny that Ctrl+M
also works after the first symbol is placed…
Oh, I forgot I implemented that. Yeah, I implemented lots of ways of doing things.
OK, now Ctrl-M will work there too, in the interest of giving the software a more square operating area.
–Mike