Hello,
I’m trying to connect to the DWM1001 chip for the first time using a Mac. I can’t seem to successfully connect to the UART Shell mode. Using the Serial app, I’m trying to send “\r” with the correct baud rate but only “@” displays on the screen.
I’ve tried using Python’s serial library and sending 0x0D to no avail. Am I using the wrong driver or did I skip a step in the setup?
It shows up how you would expect:
J-Link:
Product ID: 0x0105
Vendor ID: 0x1366
Vendor ID: 0x1366
Version: 1.00
Serial Number: 000760024898
Speed: Up to 12 Mb/sec
Manufacturer: SEGGER
Location ID: 0x14400000 / 4
And the driver information:
Name: J-Link #3
Path: /dev/cu.usbmodem1441
USB ID: 1366:0105:0100
Serial #: 760024898
Driver: AppleUSBACM (v5.0.0)
Driver ID: com.apple.driver.usb.cdc.acm