Hi,
I am using DWM3000evb + Nucleo-F429ZI. The very first example with reading the device ID has worked fine. However, I am having trouble with further examples such as ss_twr, as the code gets stuck at the dwt_checkidlerc().
Does anyone has some clue for me please?
Hi @xman236 ,
How much is the SPI frequency ? In idle rc, dwm3000 can only work with 7MHz or lower. I usually use 2MHz to communicate with dwm3000 when it is in this mode.
Best Regard,
TN
Hi @leapslabs ,
I have the same problem and setup (DWM3000evb + Nucleo-F429ZI) as OP. How exactly can I see my SPI frequency and how can I adjust it?
I already tried by
- Altering the clock dividers:
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV8;
so that remaining frequency at APB1 peiphal clocks is below 7 MHz
- I changed line 76 from simple_tx.c from
port_set_dw_ic_spi_fastrate(); to …slowrate();
The declaration is as follows:
/* @fn port_set_dw_ic_spi_slowrate
Best regard
Alex
Yeah, I am using QM33120WDK1 and I’m getting caught with the same problem.
Hi,
Can you read the device id after setting SPI to slow rate ?