I have a question regarding the component library.
I can track down my relevant component spice model and paste it into the model, but once I have set up a working symbol and prepared everything for myself, it would be nice if I could contribute to the main library of QSpice with this model. Is it possible or what is the future strategy here?
Since I’m not 100% sure about your question, I will offer two answers, one of which I hope is what you’re looking for:
If you wish to add devices to your QSPICE installation, you may right-click on the “Symbols & IP” top-level menu in the Symbol & IP Browser (use F2 to open this window if it’s not already open). From there, you may select a folder to add to the menu. It will persist across restarts of the program.
We will be adding a section to the forum where users can post models and schematics for discussion.
Yes, you can add a symbol folder outside of the QSPICE path by following my directions to Jonas (above). You’re not limited to storing symbols within the QSPICE path.
How about the output data folder? Is it possible to save schematics and output files in separate folders?
For LTSpice, I use “Microsoft OneDrive” to share my schematics between two PCs, and a local SSD to save output files. Indeed, I could share schematics by setting a local drive as a shared drive, but using “OneDrive” is more convenient for backing up files.
The only time QSPICE writes to a different folder is if you are running a schematic from a directory without write permission, like running an example in C:\Program Files\QSPICE.
That choice was made because I figured no one is spinning platters any more.
Didn’t anticipate OneDrive, which I never use as well as any cloud based anything.
Though SSD is common in new computers, lots of frugal people continue to use old HDD-based computers, also some desktop users have a 2nd or 3rd high-capacity HDD inside their computer, as well as external USB drives too. Seagate is currently sampling 30 TB hard drives plus road maps up to 50 TB, thus spinning platters is far from dead both now and years from now.
No biggie. Doesn’t change the design for QSPICE. If you spin patters, I/O is just slow. Still likely faster than the cloud – unless you put old disks in a new computer, maybe.
But in any case, in prior art, I was backward looking, wanting my software to be able to run on any old computer. I no longer get the point. QSPICE is forward looking. It’s for today’s computers and isn’t obsolete the day it is released.
I’m confused. I stumbled across this post when trying to figure out how to define the output folder. Is it still not possible to save data to a different folder?!?
I’m not sure what SSD vs spinning drive has to do with anything. I’ve never worked at a company where I’m allowed to keep data on the local drive. It needs to be accessible to everyone in the project and my local drive definitely isn’t backed up. I’m also using the same approach at home due to the simplicity of snapshots to keep my data safe.
IT would have my head if I start shuffling simulation data back and forth over the network. The only solution I can come up with is copying the simulation to the local drive and then copying it back when I’m done. Now that’s something that I definitely will mess up at some point resulting in loss of data.
I am using Microsoft OneDrive as my QSPICE working folder.
I was always shuffling my simulation data back and forth over the network! Sometimes, the “qraw” files were more than a few GB in size. Fortunately, this was on my home PC (I don’t use QSPICE for work).
Recently, I found out from the internet how to stop OneDrive from backing up specific files so that they are saved only in the local folder. I set it to skip the “QRAW” files. It seems to be working fine, and I’ll see if there are any issues.
By the way, I didn’t realize that I had to write the file extensions in UPPERCASE for the OneDrive setting.