I’m passing a Real parameter Rval via .step` in QSPICE, but my Verilog model always uses the default. I even added it as attributes but is ignored during simulation.
Has anyone successfully passed .step parameters into behavioral Verilog models?Is this even possible?
Any workaround or Verilator flag suggestions?
My Goal is to pass a real-number parameter into Verilog models from schematic testbenches while having it update across a .step sweep
I see that you’re a new user so you probably can’t upload yet…
Here’s an example showing that you can pass .step values into DLL code as both pin inputs and as attributes. Since Verilog code is compiled into a C-Block wrapper, I see no reason that it shouldn’t work in Verilog code.
Note: One issue that trips up new coders: If you generate the C/Verilog block code and subsequently modify the block (add/remove/edit ports or attributes), you must regenerate & recompile the code before running the simulation again.