Hi I wonder if there is a similar way to step models and subckt in Qspice?
I tried to replicate in Qspice but it doesn’t work (Yes I have set med Diode to Symbol Type X).
I’ve attached the example
BAV99.qsch (5.4 KB)
Hi I wonder if there is a similar way to step models and subckt in Qspice?
I tried to replicate in Qspice but it doesn’t work (Yes I have set med Diode to Symbol Type X).
I’ve attached the example
BAV99.qsch (5.4 KB)
I’m not sure if ako can function in .subckt. Let’s see if anyone has experience with that. However, why not go for the simplest method for comparing sub-circuit type diode models?
BAV99-2.qsch (7.5 KB)
It’s for tolerance/alternate analysis so it would be more neat if it’s possible too.
But yes I could do several parallel simulations too, just that it will be so many since I have multiple components to analyze together with each other.