SPICE file for TQP9111?

Was hoping to use QSpice to find correct device values for my particular band of interest.
I’d assumed the RF Amps would be available in QSpice…
May I have a Spice file for the TQP0111 in QSpice?

That should be the TPQ9111…

There is no Spice model available for the TQP9111. There are small signal s-parameters for the TQP9111 on the web here. QSpice should support s-parameters as detailed in this forum post. Typically programs like ADS or AWR are used for s-parameter simulations. You could also try Qorvo’s Match Calc program.