hello
i’m start using ss_twr example to one init node get distance of each response node
and not use PANS(it is great but unsuitble my application)
I know what i have to do is modify tx_poll,rx_poll, tx_resp,rx_resp with reference to DWM1001 system overview and 802.15.4 and figure 1, page 6 in APS016
I read the documents, but I don’t understand
just increase frame size and send group poll msg payload using tx_poll_msg?
if it is true, how set resp node seet number?
or
need any setting like framefilter?
can i get examples?
thank to read