It seems that there is a problem when I try to convert LT1009 reference voltage from LTSpice model to QSpice. The LT1009 is a 2.5V voltage reference. I havec extract this model from the LTC3.lib LTSpice library to implement it with QSpice.
The problem is, that with same schematic expected result is not identical; LTSpice returns 2.50V@25°C when QSpice gives 2.12V@25°C.
LtSpice and QSpice simulation results below:
C1 and C2 in LT1009 subckt have Rpar and Rser, which is major reason of different result between Qspice and LTspice
Here is modified .subckt based on above method LT1009_Qspice.txt (445 Bytes) LT1009.qsym (1.1 KB)
(may still have other factors contribute after modify, but not that important)