- The Issue:
Ctrl + Ltriggers the “Draw Line” tool instead of the Simulation Log. Pls advise if I have the wrong command. - The Goal: To view the results of a
.meascommand for an i-Clamp circuit. (.meas tran ScourTime TRIG I(Rclamp)=1µ rise=2 TARG I(Rclamp)=1µ fall=2) - The Setup: Using a
PULSE(0 1 0 1u 1u 10m 20m)stimulus and.tran 0 40m 0 1u. - The Problem: The “Output” (.meas tran peakval max abs(i(rclamp)):
4.9738e-17 (at Time=0.0213046)
.meas tran tau trig abs(i(rclamp))=1µ rise=1 targ abs(i(rclamp))=1µ fall=1:) while Rclamp output does appear in the Viewer
, and the “Simulation Log” is missing from the View menu.
V1
|
R1 (18k)
|
OUT
|
C1 (330n)
|
GND
Regards,