Hi,
i try to run the simple rx and tx examples and i have got multiple problems right at the start.
Im using a Qorvo DWS3000EVB on the Nordic nRF52840DK with Segger Embedded Studio 6.34a and J-Link 7.80.
I followed the instructions but when i first tried to build, i got lot of failures of missing headers and paths.
So i added them by myself. Now i can Build the examples succesfully.
One Board with the simple rx and one with the simple tx.
Now, if i want the data, ToF and all the Information for ranging, i have to read the registers. Correct?
So i need to debug via Segger embedded studio or can i use the J-Link RTT-Viewer as well?
If i try to debug, the session stops because of the HardFault_Handler.
I could press start again and it seems like it runs, but i think should get something on the debug Terminal!?
Same with the RTT Viewer.
I really don´t know exactly how i get those transmitting and receiving information, which i need for ranging.
Any Help would be great, Thanks.
Platinumer