I want to connect the DWM3000 Arduino Shield to an Arduino Board.
I cannot seem to find the library or a code example that will help me successfully connect the board to an Arduino-type board. I am wondering if any one had successfully connected and communicated with Arduino board using the DWM3000 device.
Many thanks
Thomas
To use the DWM3000 with an Arduino board, you will need to install the Arduino library for the DWM3000. You can find the library and instructions for installation on the Decawave website:
This code initializes the DWM3000 module using the Decawave library, and then reads the distance measurement in centimeters in a loop. You can use the getDistance function to retrieve the distance measurement, and you can use the other functions provided by the library to configure the DWM3000 module and perform other operations.
I hope this helps! Let me know if you have any questions.
As far as I am aware, there is no Library for the DW3000 series chip available to this date. I don’t know where Keontes information is coming from, but I did quite some research on that topic and the only “official” library was made by Makerfabs for their Arduino Shield: GitHub - Makerfabs/Makerfabs-ESP32-UWB-DW3000
Just save the “DW3000” folder in your “libraries” folder of the Arduino IDE and you should be good to go. I didn’t fully pick the library apart yet, but it seems to work quite well with other Arduino versions than the ESP32 used by makerfabs for their own PCB.