I am following gateway quick deployment guide to setup gateway via bridge node.
I have following configuration
4 anchor , 1 tag ( bridge node also act as initiator). A raspberry pi (version 3 model b) . The pins are soldered properly
I have following outputs
-
Which Raspberry Image are you using? The official one from the Release 2?
Official one DRTLS_raspbian_R2.0.img -
How do you start the DWM Daemon? Manually or just restarted the Raspberry?
Just restarted the Raspberry -
Can you get the system working or it keeps failing like this?
it keep failing like this -
Can you enter the module shell using: minicom -D /dev/serial0 (and double enter)?
yes
output:
si:
[000131.560 INF] sys: fw2 fw_ver=x01030001 cfg_ver=x00010700
[000131.560 INF] uwb0: panid=xF8AA addr=xDECAA9AF85E007B8
[000131.570 INF] mode: bn (act,-)
[000131.570 INF] uwbmac: connected
[000131.580 INF] enc: off
[000131.580 INF] ble: addr=C2:7A:7F:A8:9E:E4
la
[000127.710 INF] AN: cnt=3 seq=x08
[000127.710 INF] 0) id=DECA50A194214D33 seat=0 seens=161 rssi=-82
[000127.720 INF] 1) id=DECAD61017C593A7 seat=4 seens=161 rssi=-82
[000127.730 INF] 2) id=DECA0D4B4613970F seat=5 seens=160 rssi=-80
[000127.730 INF]
Why only three anchor are listed , Bridge node is not listed as an anchor?
-
Please send outputs of the commands on the failing system:
-
lsmod
Module Size Used by
fuse 106496 3
rfcomm 49152 6
cmac 16384 1
bnep 20480 2
hci_uart 36864 1
btbcm 16384 1 hci_uart
serdev 20480 1 hci_uart
bluetooth 368640 29 hci_uart,bnep,btbcm,rfcomm
ecdh_generic 28672 1 bluetooth
spidev 16384 0
brcmfmac 307200 0
brcmutil 16384 1 brcmfmac
snd_bcm2835 32768 1
cfg80211 573440 1 brcmfmac
rfkill 28672 6 bluetooth,cfg80211
snd_pcm 98304 1 snd_bcm2835
snd_timer 32768 1 snd_pcm
snd 69632 5 snd_timer,snd_bcm2835,snd_pcm
spi_bcm2835 16384 0
evdev 24576 8
joydev 20480 0
uio_pdrv_genirq 16384 0
uio 20480 1 uio_pdrv_genirq
fixed 16384 0
dwm 77824 4
i2c_dev 16384 0
ip_tables 24576 0
x_tables 32768 1 ip_tables
ipv6 434176 57 -
ls -la /dev/dwm0
crw------- 1 root root 200, 0 Oct 9 16:39 /dev/dwm0 -
ps ax | grep dwm
492 ? Sl 0:00 /usr/local/bin/dwm-daemon -c /etc/dwm1001/dwm1001.config -l /var/log/dwm-daemon.log
496 ? Sl 0:00 /usr/local/bin/dwm-proxy -c /etc/dwm1001/dwm1001-proxy.config
1553 pts/1 S+ 0:00 grep --color=auto dwm -
config file
config file
DWM Kernel Module settings
UWB network PANID
Allowed values: 16-bit number in decimal, hexadecimal or octal format
panid = 0xF8AA
UWB encryption
Allowed values: true/false
enc_en = false
UWB encryption key
Allowed values: 128-bit number in hexadecimal format
enc_key = “11111111222222223333333344444444”
uwb_fwup = true
UWB mode
Allowed values: 0=Off 1=Passive 2=Active
uwb_mode = 2
daemon settings
proxy_server_host = “localhost”
proxy_server_port = 1885
mqtt_user = “dwmuser”
mqtt_password = “dwmpass”
mqtt_topic_prefix = “dwm”
- dmesg
0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.50-v7+ (dc4@dc4-XPS13-9333) (gcc version 4.9.3 (crosstool-NG crosstool-ng-1.22.0-88-g8460611)) #1122 SMP Tue Jun 19 12:26:26 BST 2018
[ 0.000000] CPU: ARMv7 Processor [410fd034] revision 4 (ARMv7), cr=10c5383d
[ 0.000000] CPU: div instructions available: patching division code
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Raspberry Pi 3 Model B Rev 1.2
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] cma: Reserved 8 MiB at 0x3ac00000
[ 0.000000] On node 0 totalpages: 242688
[ 0.000000] free_area_init_node: node 0, pgdat 80c85000, node_mem_map ba3a1000
[ 0.000000] Normal zone: 2133 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 242688 pages, LIFO batch:31
[ 0.000000] percpu: Embedded 17 pages/cpu @ba34a000 s38720 r8192 d22720 u69632
[ 0.000000] pcpu-alloc: s38720 r8192 d22720 u69632 alloc=17*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 240555
[ 0.000000] Kernel command line: 8250.nr_uarts=1 bcm2708_fb.fbwidth=1824 bcm2708_fb.fbheight=984 bcm2708_fb.fbswap=1 vc_mem.mem_base=0x3ec00000 vc_mem.mem_size=0x40000000 dwc_otg.lpm_enable=0 console=tty1 root=PARTUUID=c049f471-02 rootfstype=ext4 elevator=deadline fsck.repair=yes rootwait quiet splash plymouth.ignore-serial-consoles
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 940236K/970752K available (7168K kernel code, 575K rwdata, 2072K rodata, 1024K init, 706K bss, 22324K reserved, 8192K cma-reserved)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xbb800000 - 0xff800000 (1088 MB)
lowmem : 0x80000000 - 0xbb400000 ( 948 MB)
modules : 0x7f000000 - 0x80000000 ( 16 MB)
.text : 0x80008000 - 0x80800000 (8160 kB)
.init : 0x80b00000 - 0x80c00000 (1024 kB)
.data : 0x80c00000 - 0x80c8fef4 ( 576 kB)
.bss : 0x80c96f40 - 0x80d478b4 ( 707 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] ftrace: allocating 25253 entries in 75 pages
[ 0.000000] Hierarchical RCU implementation.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] arch_timer: cp15 timer(s) running at 19.20MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x46d987e47, max_idle_ns: 440795202767 ns
[ 0.000007] sched_clock: 56 bits at 19MHz, resolution 52ns, wraps every 4398046511078ns
[ 0.000018] Switching to timer-based delay loop, resolution 52ns
[ 0.000263] Console: colour dummy device 80x30
[ 0.000281] console [tty1] enabled
[ 0.000309] Calibrating delay loop (skipped), value calculated using timer frequency… 38.40 BogoMIPS (lpj=192000)
[ 0.000325] pid_max: default: 32768 minimum: 301
[ 0.000643] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000657] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001588] Disabling memory control group subsystem
[ 0.001669] CPU: Testing write buffer coherency: ok
[ 0.002060] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002438] Setting up static identity map for 0x100000 - 0x10003c
[ 0.002555] Hierarchical SRCU implementation.
[ 0.003187] smp: Bringing up secondary CPUs …
[ 0.003864] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.004608] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.005337] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.005440] smp: Brought up 1 node, 4 CPUs
[ 0.005451] SMP: Total of 4 processors activated (153.60 BogoMIPS).
[ 0.005457] CPU: All CPU(s) started in HYP mode.
[ 0.005461] CPU: Virtualization extensions available.
[ 0.006316] devtmpfs: initialized
[ 0.016217] random: get_random_u32 called from bucket_table_alloc+0xfc/0x24c with crng_init=0
[ 0.016945] VFP support v0.3: implementor 41 architecture 3 part 40 variant 3 rev 4
[ 0.017166] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.017184] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.017745] pinctrl core: initialized pinctrl subsystem
[ 0.018484] NET: Registered protocol family 16
[ 0.021178] DMA: preallocated 1024 KiB pool for atomic coherent allocations
[ 0.026021] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.026028] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.026226] Serial: AMBA PL011 UART driver
[ 0.027841] bcm2835-mbox 3f00b880.mailbox: mailbox enabled
[ 0.028296] uart-pl011 3f201000.serial: could not find pctldev for node /soc/gpio@7e200000/uart0_pins, deferring probe
[ 0.060125] bcm2835-dma 3f007000.dma: DMA legacy API manager at bb813000, dmachans=0x1
[ 0.061536] SCSI subsystem initialized
[ 0.061760] usbcore: registered new interface driver usbfs
[ 0.061817] usbcore: registered new interface driver hub
[ 0.061902] usbcore: registered new device driver usb
[ 0.070090] raspberrypi-firmware soc:firmware: Attached to firmware from 2018-06-07 15:31
[ 0.071465] clocksource: Switched to clocksource arch_sys_counter
[ 0.148517] VFS: Disk quotas dquot_6.6.0
[ 0.148602] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.148788] FS-Cache: Loaded
[ 0.148986] CacheFiles: Loaded
[ 0.157733] NET: Registered protocol family 2
[ 0.158452] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.158562] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.158748] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.158877] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.158921] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.159148] NET: Registered protocol family 1
[ 0.159586] RPC: Registered named UNIX socket transport module.
[ 0.159592] RPC: Registered udp transport module.
[ 0.159597] RPC: Registered tcp transport module.
[ 0.159602] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.161116] hw perfevents: enabled with armv7_cortex_a7 PMU driver, 7 counters available
[ 0.163924] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.171905] FS-Cache: Netfs ‘nfs’ registered for caching
[ 0.172493] NFS: Registering the id_resolver key type
[ 0.172523] Key type id_resolver registered
[ 0.172528] Key type id_legacy registered
[ 0.172543] nfs4filelayout_init: NFSv4 File Layout Driver Registering…
[ 0.174411] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 251)
[ 0.174533] io scheduler noop registered
[ 0.174540] io scheduler deadline registered (default)
[ 0.174812] io scheduler cfq registered
[ 0.174819] io scheduler mq-deadline registered
[ 0.174825] io scheduler kyber registered
[ 0.177492] BCM2708FB: allocated DMA memory fad10000
[ 0.177518] BCM2708FB: allocated DMA channel 0 @ bb813000
[ 0.227648] Console: switching to colour frame buffer device 228x61
[ 0.257006] Serial: 8250/16550 driver, 1 ports, IRQ sharing enabled
[ 0.258401] bcm2835-rng 3f104000.rng: hwrng registered
[ 0.258539] vc-mem: phys_addr:0x00000000 mem_base=0x3ec00000 mem_size:0x40000000(1024 MiB)
[ 0.259013] vc-sm: Videocore shared memory driver
[ 0.259293] gpiomem-bcm2835 3f200000.gpiomem: Initialised: Registers at 0x3f200000
[ 0.268965] brd: module loaded
[ 0.277886] loop: module loaded
[ 0.277901] Loading iSCSI transport class v2.0-870.
[ 0.278582] libphy: Fixed MDIO Bus: probed
[ 0.278685] usbcore: registered new interface driver lan78xx
[ 0.278743] usbcore: registered new interface driver smsc95xx
[ 0.278759] dwc_otg: version 3.00a 10-AUG-2012 (platform bus)
[ 0.506889] Core Release: 2.80a
[ 0.506898] Setting default values for core params
[ 0.506933] Finished setting default values for core params
[ 0.707203] Using Buffer DMA mode
[ 0.707209] Periodic Transfer Interrupt Enhancement - disabled
[ 0.707215] Multiprocessor Interrupt Enhancement - disabled
[ 0.707221] OTG VER PARAM: 0, OTG VER FLAG: 0
[ 0.707234] Dedicated Tx FIFOs mode
[ 0.707637] WARN::dwc_otg_hcd_init:1046: FIQ DMA bounce buffers: virt = 0xbad04000 dma = 0xfad04000 len=9024
[ 0.707666] FIQ FSM acceleration enabled for :
Non-periodic Split Transactions
Periodic Split Transactions
High-Speed Isochronous Endpoints
Interrupt/Control Split Transaction hack enabled
[ 0.707674] dwc_otg: Microframe scheduler enabled
[ 0.707730] WARN::hcd_init_fiq:459: FIQ on core 1 at 0x805e7d20
[ 0.707741] WARN::hcd_init_fiq:460: FIQ ASM at 0x805e8088 length 36
[ 0.707754] WARN::hcd_init_fiq:486: MPHI regs_base at 0xbb87e000
[ 0.707812] dwc_otg 3f980000.usb: DWC OTG Controller
[ 0.707846] dwc_otg 3f980000.usb: new USB bus registered, assigned bus number 1
[ 0.707879] dwc_otg 3f980000.usb: irq 62, io mem 0x00000000
[ 0.707927] Init: Port Power? op_state=1
[ 0.707932] Init: Power Port (0)
[ 0.708137] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 0.708148] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 0.708156] usb usb1: Product: DWC OTG Controller
[ 0.708164] usb usb1: Manufacturer: Linux 4.14.50-v7+ dwc_otg_hcd
[ 0.708172] usb usb1: SerialNumber: 3f980000.usb
[ 0.708796] hub 1-0:1.0: USB hub found
[ 0.708844] hub 1-0:1.0: 1 port detected
[ 0.709397] dwc_otg: FIQ enabled
[ 0.709402] dwc_otg: NAK holdoff enabled
[ 0.709408] dwc_otg: FIQ split-transaction FSM enabled
[ 0.709417] Module dwc_common_port init
[ 0.709656] usbcore: registered new interface driver usb-storage
[ 0.709823] mousedev: PS/2 mouse device common for all mice
[ 0.709896] IR NEC protocol handler initialized
[ 0.709902] IR RC5(x/sz) protocol handler initialized
[ 0.709907] IR RC6 protocol handler initialized
[ 0.709912] IR JVC protocol handler initialized
[ 0.709917] IR Sony protocol handler initialized
[ 0.709922] IR SANYO protocol handler initialized
[ 0.709928] IR Sharp protocol handler initialized
[ 0.709933] IR MCE Keyboard/mouse protocol handler initialized
[ 0.709938] IR XMP protocol handler initialized
[ 0.710647] bcm2835-wdt 3f100000.watchdog: Broadcom BCM2835 watchdog timer
[ 0.710906] bcm2835-cpufreq: min=600000 max=1200000
[ 0.711276] sdhci: Secure Digital Host Controller Interface driver
[ 0.711280] sdhci: Copyright(c) Pierre Ossman
[ 0.711676] mmc-bcm2835 3f300000.mmc: could not get clk, deferring probe
[ 0.711994] sdhost-bcm2835 3f202000.mmc: could not get clk, deferring probe
[ 0.712091] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.713496] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.713676] hidraw: raw HID events driver (C) Jiri Kosina
[ 0.713804] usbcore: registered new interface driver usbhid
[ 0.713809] usbhid: USB HID core driver
[ 0.714568] vchiq: vchiq_init_state: slot_zero = bad80000, is_master = 0
[ 0.716089] [vc_sm_connected_init]: start
[ 0.725621] [vc_sm_connected_init]: end - returning 0
[ 0.726224] Initializing XFRM netlink socket
[ 0.726247] NET: Registered protocol family 17
[ 0.726348] Key type dns_resolver registered
[ 0.726861] Registering SWP/SWPB emulation handler
[ 0.727452] registered taskstats version 1
[ 0.733424] uart-pl011 3f201000.serial: cts_event_workaround enabled
[ 0.733510] 3f201000.serial: ttyAMA0 at MMIO 0x3f201000 (irq = 87, base_baud = 0) is a PL011 rev2
[ 0.735067] 3f215040.serial: ttyS0 at MMIO 0x0 (irq = 166, base_baud = 31250000) is a 16550
[ 0.735951] mmc-bcm2835 3f300000.mmc: mmc_debug:0 mmc_debug2:0
[ 0.735960] mmc-bcm2835 3f300000.mmc: DMA channel allocated
[ 0.792118] sdhost: log_buf @ bad07000 (fad07000)
[ 0.826807] mmc1: queuing unknown CIS tuple 0x80 (2 bytes)
[ 0.828375] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
[ 0.829942] mmc1: queuing unknown CIS tuple 0x80 (3 bytes)
[ 0.832747] mmc1: queuing unknown CIS tuple 0x80 (7 bytes)
[ 0.871483] mmc0: sdhost-bcm2835 loaded - DMA enabled (>1)
[ 0.872544] of_cfs_init
[ 0.872686] of_cfs_init: OK
[ 0.873267] Waiting for root device PARTUUID=c049f471-02…
[ 0.908709] random: fast init done
[ 0.921563] Indeed it is in host mode hprt0 = 00021501
[ 1.008018] mmc1: new high speed SDIO card at address 0001
[ 1.049817] mmc0: host does not support reading read-only switch, assuming write-enable
[ 1.053625] mmc0: new high speed SDXC card at address aaaa
[ 1.054072] mmcblk0: mmc0:aaaa SD64G 59.5 GiB
[ 1.055965] mmcblk0: p1 p2
[ 1.083559] EXT4-fs (mmcblk0p2): INFO: recovery required on readonly filesystem
[ 1.083567] EXT4-fs (mmcblk0p2): write access will be enabled during recovery
[ 1.131511] usb 1-1: new high-speed USB device number 2 using dwc_otg
[ 1.131635] Indeed it is in host mode hprt0 = 00001101
[ 1.371757] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 1.371771] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 1.372483] hub 1-1:1.0: USB hub found
[ 1.372563] hub 1-1:1.0: 5 ports detected
[ 1.691573] usb 1-1.1: new high-speed USB device number 3 using dwc_otg
[ 1.821748] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 1.821764] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 1.824525] smsc95xx v1.0.6
[ 1.862513] EXT4-fs (mmcblk0p2): recovery complete
[ 1.864551] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 1.864611] VFS: Mounted root (ext4 filesystem) readonly on device 179:2.
[ 1.872256] devtmpfs: mounted
[ 1.875398] Freeing unused kernel memory: 1024K
[ 1.914634] smsc95xx 1-1.1:1.0 eth0: register ‘smsc95xx’ at usb-3f980000.usb-1.1, smsc95xx USB 2.0 Ethernet, b8:27:eb:92:6b:bf
[ 2.231566] usb 1-1.2: new full-speed USB device number 4 using dwc_otg
[ 2.248464] systemd[1]: System time before build time, advancing clock.
[ 2.378816] NET: Registered protocol family 10
[ 2.380172] Segment Routing with IPv6
[ 2.389627] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 2.395886] usb 1-1.2: New USB device found, idVendor=3151, idProduct=1002
[ 2.395901] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 2.395910] usb 1-1.2: Product: Wireless Device
[ 2.395918] usb 1-1.2: Manufacturer: YICHIP
[ 2.405396] hid-generic 0003:3151:1002.0001: hiddev96,hidraw0: USB HID v2.00 Device [YICHIP Wireless Device] on usb-3f980000.usb-1.2/input0
[ 2.406986] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.418491] systemd[1]: systemd 232 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD +IDN)
[ 2.419092] systemd[1]: Detected architecture arm.
[ 2.420095] systemd[1]: Set hostname to .
[ 2.426744] input: YICHIP Wireless Device as /devices/platform/soc/3f980000.usb/usb1/1-1/1-1.2/1-1.2:1.1/0003:3151:1002.0002/input/input0
[ 2.453647] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.475563] random: systemd-cryptse: uninitialized urandom read (16 bytes read)
[ 2.492362] hid-generic 0003:3151:1002.0002: input,hiddev97,hidraw1: USB HID v2.00 Mouse [YICHIP Wireless Device] on usb-3f980000.usb-1.2/input1
[ 2.863077] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 2.863813] systemd[1]: Listening on Journal Socket.
[ 2.864634] systemd[1]: Created slice User and Session Slice.
[ 2.865215] systemd[1]: Created slice System Slice.
[ 2.865378] systemd[1]: Reached target Slices.
[ 2.868506] systemd[1]: Mounting Debug File System…
[ 2.873825] systemd[1]: Starting Set the console keyboard layout…
[ 2.952064] i2c /dev entries driver
[ 2.959030] dwm: no symbol version for module_layout
[ 2.959058] dwm: loading out-of-tree module taints kernel.
[ 3.347175] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 3.456281] systemd-journald[98]: Received request to flush runtime journal from PID 1
[ 3.811283] dwm spi0.0: loading
[ 3.811632] dwm spi0.0: DWM1001 TWR Real Time Location System
[ 3.811643] dwm spi0.0:
[ 3.811650] dwm spi0.0: Copyright : 2016-2019 LEAPS and Decawave
[ 3.811659] dwm spi0.0: License : Please visit Decawave is now part of Qorvo
[ 3.811666] dwm spi0.0: Compiled : Feb 4 2019 12:36:58
[ 3.962082] snd_bcm2835: module is from the staging directory, the quality is unknown, you have been warned.
[ 3.968430] bcm2835_alsa bcm2835_alsa: card created with 8 channels
[ 4.142153] brcmfmac: F1 signature read @0x18000000=0x1541a9a6
[ 4.151975] brcmfmac: brcmf_fw_map_chip_to_name: using brcm/brcmfmac43430-sdio.bin for chip 0x00a9a6(43430) rev 0x000001
[ 4.152270] usbcore: registered new interface driver brcmfmac
[ 4.182670] dwm spi0.0: invalid bridge config detected = 0x2816
[ 4.182686] dwm spi0.0: configuring bridge …
[ 4.285908] dwm spi0.0: reseting bridge
[ 4.530657] brcmfmac: brcmf_c_preinit_dcmds: Firmware version = wl0: Oct 23 2017 03:55:53 version 7.45.98.38 (r674442 CY) FWID 01-e58d219f
[ 4.531989] brcmfmac: brcmf_c_preinit_dcmds: CLM version = API: 12.2 Data: 7.11.15 Compiler: 1.24.2 ClmImport: 1.24.1 Creation: 2014-05-26 10:53:55 Inc Data: 9.10.39 Inc Compiler: 1.29.4 Inc ClmImport: 1.36.3 Creation: 2017-10-23 03:47:14
[ 4.701559] usb 1-1.4: new low-speed USB device number 5 using dwc_otg
[ 4.848528] usb 1-1.4: New USB device found, idVendor=046d, idProduct=c31d
[ 4.848548] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 4.848557] usb 1-1.4: Product: USB Keyboard
[ 4.848565] usb 1-1.4: Manufacturer: Logitech
[ 4.873573] input: Logitech USB Keyboard as /devices/platform/soc/3f980000.usb/usb1/1-1/1-1.4/1-1.4:1.0/0003:046D:C31D.0003/input/input1
[ 4.954228] hid-generic 0003:046D:C31D.0003: input,hidraw2: USB HID v1.10 Keyboard [Logitech USB Keyboard] on usb-3f980000.usb-1.4/input0
[ 4.977756] input: Logitech USB Keyboard as /devices/platform/soc/3f980000.usb/usb1/1-1/1-1.4/1-1.4:1.1/0003:046D:C31D.0004/input/input2
[ 5.043395] hid-generic 0003:046D:C31D.0004: input,hidraw3: USB HID v1.10 Device [Logitech USB Keyboard] on usb-3f980000.usb-1.4/input1
[ 5.351572] dwm spi0.0: bridge ok
[ 5.427759] uart-pl011 3f201000.serial: no DMA platform data
[ 5.658699] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
[ 5.658879] brcmfmac: power management disabled
[ 6.023759] smsc95xx 1-1.1:1.0 eth0: hardware isn’t capable of remote wakeup
[ 6.024189] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 6.435873] IPv6: ADDRCONF(NETDEV_CHANGE): wlan0: link becomes ready
[ 7.529788] Adding 102396k swap on /var/swap. Priority:-2 extents:1 across:102396k SSFS
[ 8.127876] dwm spi0.0: PAN ID changed by user to xF8AA
[ 8.127893] dwm spi0.0: encryption key changed by user
[ 8.127902] dwm spi0.0: encryption configuration changed by user
[ 8.127911] dwm spi0.0: firmware update configuration changed by user
[ 8.127918] dwm spi0.0: UWB mode configuration changed by user
[ 8.127927] dwm spi0.0: reinitialize …
[ 10.034709] Bluetooth: Core ver 2.22
[ 10.034792] NET: Registered protocol family 31
[ 10.034798] Bluetooth: HCI device and connection manager initialized
[ 10.034818] Bluetooth: HCI socket layer initialized
[ 10.034832] Bluetooth: L2CAP socket layer initialized
[ 10.034867] Bluetooth: SCO socket layer initialized
[ 10.047817] Bluetooth: HCI UART driver ver 2.3
[ 10.047838] Bluetooth: HCI UART protocol H4 registered
[ 10.047845] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 10.048062] Bluetooth: HCI UART protocol Broadcom registered
[ 10.175140] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 10.175149] Bluetooth: BNEP filters: protocol multicast
[ 10.175167] Bluetooth: BNEP socket layer initialized
[ 10.244718] Bluetooth: RFCOMM TTY layer initialized
[ 10.244741] Bluetooth: RFCOMM socket layer initialized
[ 10.244761] Bluetooth: RFCOMM ver 1.11
[ 10.595566] usb 1-1.5: new low-speed USB device number 6 using dwc_otg
[ 10.726491] usb 1-1.5: New USB device found, idVendor=093a, idProduct=2510
[ 10.726503] usb 1-1.5: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 10.726508] usb 1-1.5: Product: USB Optical Mouse
[ 10.726512] usb 1-1.5: Manufacturer: PixA琀
[ 10.730867] input: PixA琀 USB Optical Mouse as /devices/platform/soc/3f980000.usb/usb1/1-1/1-1.5/1-1.5:1.0/0003:093A:2510.0005/input/input3
[ 10.731350] hid-generic 0003:093A:2510.0005: input,hidraw4: USB HID v1.11 Mouse [PixA琀 USB Optical Mouse] on usb-3f980000.usb-1.5/input0
[ 11.506263] dwm spi0.0: setting bridge PAN ID to xF8AA …
[ 11.561528] dwm spi0.0: setting encryption key on gateway
[ 11.692678] dwm spi0.0: invalid bridge config detected = 0x2812
[ 11.692694] dwm spi0.0: configuring bridge …
[ 11.796085] dwm spi0.0: reseting bridge
[ 12.101533] usb 1-1.5: reset low-speed USB device number 6 using dwc_otg
[ 12.401516] usb 1-1.5: device descriptor read/64, error -32
[ 12.582861] fuse init (API version 7.26)
[ 12.871509] dwm spi0.0: bridge ok
[ 24.625141] random: crng init done
[ 24.625157] random: 7 urandom warning(s) missed due to ratelimiting
[ 180.602809] dwm spi0.0: expected tlv type 113 != 0
[ 180.602825] dwm spi0.0: bh_ul_decode_tlv rv(-3)
[ 180.602833] dwm spi0.0: uplink discarded, sfn=63
[ 213.002655] dwm spi0.0: expected tlv type 114 != 242
[ 213.002664] dwm spi0.0: bh_ul_decode_tlv rv(-3)
[ 213.002669] dwm spi0.0: uplink discarded, sfn=387
[ 216.202699] dwm spi0.0: expected tlv type 114 != 242
[ 216.202712] dwm spi0.0: bh_ul_decode_tlv rv(-3)
[ 216.202716] dwm spi0.0: uplink discarded, sfn=419
[ 233.792816] dwm spi0.0: expected tlv type 113 != 241
[ 233.792826] dwm spi0.0: bh_ul_decode_tlv rv(-3)
[ 233.792831] dwm spi0.0: uplink discarded, sfn=595
[ 235.500737] dwm spi0.0: uplink len=68 do not fit into len=3 * cnt=1
[ 235.500751] dwm spi0.0: error -12 in state=1
[ 235.500757] dwm spi0.0: reinitialize …
[ 238.882619] dwm spi0.0: decode TLV failed, error 3 t:192 l:1
[ 238.882638] dwm spi0.0: dwm_status_get failed, error -12
[ 238.882644] dwm spi0.0: reseting bridge
[ 239.991544] dwm spi0.0: bridge can’t be initialized, error -14
[ 243.392604] dwm spi0.0: bridge is not connected to UWB network
[ 243.392616] dwm spi0.0: bridge ok
Can anyone help me with proper instruction and guide me to install the gatewat