Since this is my first post here, I would like thank you so much for making Qspice available for free.
Now to my question: I’ve been playing around with Ø-Devices and trying to set the output impedance (instance parameter ROUT), which works, except for setting it to zero, which seems to do nothing. I have to set it to 1e-308, which is probably good enough, but being able to set it to actual zero would be nicer.
The output is going to be a Norton equivalent circuit. It’s impedance can not be zero. QSPICE is trying to be polite by ignoring a request to set it to zero.
Norton equivalents are always preferred in circuit simulation because of the way the rest of the circuit is represented.