Seat allotted to anchors can be fixed?

Hi,
I am working on DWM1001 DEV for Forklift tracking . As the limitation of anchors due to PANS FW v2 is 30, but that is scalable by considering some rules.
I have query regarding Seat allocation

  1. As i am using around 200 anchors in an area then can the seat allotted to anchors will remain same after setting up the anchors setup, because they will remain power up all the time?
  2. If i deploy anchors in two areas having same n/w id but areas in which they are deployed are quite far from each other the do i need to make initiator in both areas?
    Because there is not ranging between areas.
    Please reply for the above queries.
    Regards
    Akansha