Hello,
I am using all the required configurations so that I have Standard Short (8-symbol) SFD. I need to adjust the RXPACC value by SFD. In Table 18 in the user manual of dw1000, the sequence for this case is written as “0+0-+00-”.
My question is if this sequence is just an example and my sequence in my program may be different or if I am using all the configurations for Standard Short (8-symbol) (standard IEEE 8-symbol SFD) then the SFD sequence is the same as “0+0-+00-” and I can use “-5” as my adjustment value?
Thanks for your help in advance