This is normal behavior. You cannot range between TREK ARM tag application and DecaRanging PC anchor. The TREK tag timings are optimised, the turnaround times are too quick for the PC application.
If you need an ARM application tag, then you must use EVK1000 ARM SW in the EVB1000.
I am just getting started on EVK1000 and I have the same issue.
“When I flash the latest Deca Ranging 3.05 application to the boards, the Deca Ranging application works.” Could you elaborate on this? I would like for Deca Ranging application to work, so how do I go about this?
Hi,
What Software version is on the boards? It will tell the version when resetting the board on the LCD. is it version 2.35, 3.05 or 2.10
Also what version of the PC Decaranging are you using? 3.05 or 2.58.
And when you connect the EVB1000 to the PC are the drivers installed? (see device manager ports (COM & LPT)
/Leo
Hi please make sure, that the tag and anchor are using the same configuration, eg, speed rate, channel…, as the decive connected to the PC will get a default configuration automacally, so the other one should by troggling the corresponding switch get the same configuration.