RFSW8008 Absolute Maximum Ratings Specifications

Hi all,

I have some questions regarding the RFSW8008 absolute maximum ratings and specifications.

  1. What are the absolute maximum ratings for each of the ANT and RF1/2 pins?
  2. Are there any concerns when using it with 802.11ax (5 GHz band only)?

Best regards
sss

The max rating isn’t specified in the datasheet, but it will be around 27dBm (CW into 50R) with 1.8V control logic, and 29dBm with 3.6V.
There are no concerns using with 11ax in the 5GHz band. This is specified in the datasheet, you can get linear output power of 21dBm with EVM -40dB max with 3.6V control logic.