Hi, I would like to have the following RF data on RFFC5072 mixer IC with integrated synthesizer:
- RF-IF and LO-IF isolation when the IC is used in downconversion mode. The RF frequency range is 2030MHz to 3GHz, while LO is set to 2GHz. This will set the IF frequency range from 30MHz to 1GHz.
- Synthesizer phase noise from 1KHz offset to 20MHz offset when LO is set to 2GHz and 52MHz crystal oscillator is used.
- On page 2 of the datasheet, it says that the typical mixer conversion gain driving a 4:1 balun at the output is -2dB. However, on page 21, the conversion gain plot shows -5dB loss at 2GHz. What is the expected mixer conversion gain for 2GHz to 3GHz RF frequency at the input port when the recommended 4:1 balen is used at the output port?
- Mixer spur table listing all spur levels for the operating conditions given in #1.
Thanks,
Noman