If a new symbol is created, is there any way to refresh the symbol list in current schematic?
Currently I have to remove and add the path again or close current schematic and reopen it. Is there a shortcut to refresh it?
1 Like
Except for the Builtin Symbols, you don’t really need the Symbol & IP Browser.
You can just use Windows File Explorer. Just drag a symbol file onto the schematic.
It’s the reason you want to install as Admin, so you get a preview of the symbol in Windows File Explorer.
–Mike
1 Like
@KSKelvin
Hello Kelvin,
I am having the same discomfort with the “symbol & IP”. A refresh button would be really appreciated.
Was this addressed in August 2023?
No refresh
… what I do is close and re-open Qspice. Eventually I get used to this.
Hey Kelvin,
Just noticed that you can right-click on the directory, chose Edit User-Supplied Directory and click Ok. It refreshes all directories.
2 Likes
Thanks for sharing this trick!