Hello,
I was wondering if it is possible to change the function of one of the buttons on the DWM1001 module (SW1 or SW2), and if it is, where in the source code I could go to change it.
If I can’t change the function of either button, where should I connect an external button?
Thanks!
Hi Izzy,
Please see the doc below, section 7:
You can reprogram SW2 if you don’t need the ble wake up functionality.
Otherwise you can add a new button on the gpios. You can access them on the header J7 on the deb board.
Thank you,
Regards
Yves
Thanks! Where exactly in the source code could I reconfigure SW2?
you did it ? what source code used ?